VideoLibrary

A breadboard power supply with USB C power delivery - The Byte Sized Engineer | DigiKey

Most breadboard power supplies use a DC barrel jack or USB mini connectors. But let’s be honest, most of our workbenches are now equipped with USB C power supplies which can offer a lot of benefits. In this video Zach updates and improves his old breadboard power supply with a new PCB that uses USB C power delivery. This means he can select voltages between 3.3V, 5V, 9V, 12V, 15V, and 20V on each rail of the breadboard.

How to build a solder reflow oven https://youtu.be/asZ1zhef8Ss?si=aRIjn7XVy-kfsZrs

Bill of materials CYPD3177 https://www.digikey.com/short/3r4wttt9 CY4533 EVAL https://www.digikey.com/short/qwj5v9v4 USB C PD wall adapter https://www.digikey.com/short/p4c9dp7t MHP30 mini hot plate https://www.digikey.com/short/n1ph0p77

Byte Sized Engineer channel - https://www.youtube.com/@bytesizedengineering Maker.io - https://www.digikey.com/en/maker Digi-Key’s Blog – TheCircuit https://www.digikey.com/en/blog Connect with Digi-Key on Facebook https://www.facebook.com/digikey.electronics/ And follow us on Twitter https://twitter.com/digikey

Video Chapters: 00:00 Introduction 00:37 The pros and cons of existing power supplies 01:14 Benefits of using USB C 02:04 Finding the right IC 02:30 Designing the PCB 03:04 Using the stencil to apply solder paste 03:58 Placing components on the board 04:16 Reflowing board using mini hot plate 04:40 Printing an enclosure 05:18 Testing everything out for the first time 06:01 What I want to improve on this first version

6/17/2024 5:07:39 PM

Part List

ImagemNúmero de peça do fabricanteDescriçãoAvailable QuantityPreçoVer detalhes
IC USB TYPE-C PORT CONTROL 24QFNCYPD3177-24LQXQTIC USB TYPE-C PORT CONTROL 24QFN7358 - Immediate$1.76Ver detalhes
MINIWARE MHP30 MINI HOT PLATE PRFIT0888MINIWARE MHP30 MINI HOT PLATE PR29 - Immediate$113.67Ver detalhes
AC/DC WALL MNT ADAPT 5V-20V 60WQFWC-60-20-USCRAC/DC WALL MNT ADAPT 5V-20V 60W111 - Immediate$23.07Ver detalhes
EVAL BOARD FOR CYPD3177CY4533EVAL BOARD FOR CYPD3177319 - Immediate$21.26Ver detalhes