Maker.io main logo

Intro to ROS Part 2: Getting Started with ROS 2 Using the Command Line

779

2025-09-18 | By ShawnHymel

Raspberry Pi SBC

In this tutorial, we’ll dive into one of the most essential parts of working with ROS 2: the command-line interface (CLI). Before writing any code, it’s important to understand the basic tools that ROS 2 provides for exploring, debugging, and interacting with nodes, topics, and services. These tools will be invaluable when you're developing and testing your own robotic applications.

Prerequisites: You should have a ROS 2 development environment ready. If you're following along with our series, we’ll be using a Docker image with ROS 2 Jazzy pre-installed. You can view the Docker setup instructions here: https://github.com/ShawnHymel/introduction-to-ros

What Are ROS 2 Nodes, Topics, and Services?

Intro to ROS Part 2: Getting Started with ROS 2 Using the Command Line

ROS (Robot Operating System) is a middleware that allows you to write modular, scalable robotics applications. Three of the most fundamental building blocks in ROS 2 are:

  • Nodes: Self-contained processes that perform specific functions. Think of them as the fundamental building blocks of your robot software, where each node performs a distinct job, such as reading a sensor, processing an image, or controlling a motor.
  • Topics: Named communication channels for publishing/subscribing to data streams. Topics are ideal for continuous data exchange, like streaming sensor data or broadcasting commands.
  • Services: Synchronous request/response interfaces for direct communication. Use services when you need a one-off command that expects a reply, such as querying the robot's battery level or sending it to a specific location.

Understanding how to monitor and interact with these using the CLI is a critical skill. These tools let you visualize node communication, diagnose errors, and simulate communication patterns without writing any code.

Running ROS 2 in Docker

To start, download the GitHub repository from: https://github.com/ShawnHymel/introduction-to-ros. You can do this by clicking Code > Download ZIP file or by using the git command line tool (if you have it installed on your system):

git clone https://github.com/ShawnHymel/introduction-to-ros

Navigate into the repository’s directory and build the Docker image:

Copy Code
cd introduction-to-ros 
docker build -t env-ros2 .

Start the Docker container that contains your ROS 2 environment. On macOS or Linux, run:

Copy Code
docker run --rm -it \
 -e PUID=$(id -u) \ 
 -e PGID=$(id -g) \ 
 -p 22002:22 \ 
 -p 3000:3000 \
 -v "${PWD}/workspace:/config/workspace" \
 env-ros2

On Windows (PowerShell):

Copy Code
docker run --rm -it \
 -e PUID=$(wsl id -u) \
 -e PGID=$(wsl id -g) \
 -p 22002:22 \
 -p 3000:3000 \
 -v "${PWD}\workspace:/config/workspace" \ 
env-ros2

Open a browser and navigate to localhost:3000. All your custom code will be stored in the workspace directory. Note that this directory is mapped to your host operating system, so any work you do in the ROS environment will be saved on your computer.

Verifying the ROS 2 Environment

To check that everything is working, open a terminal in the container and run:

Copy Code
ros2

You should see a list of ROS 2 subcommands, such as topic, service, node, and run. This confirms that ROS 2 is installed and correctly sourced.

If you’re using a system where ROS 2 isn’t automatically sourced, you can run:

Copy Code
source /opt/ros/jazzy/setup.bash

This step ensures that the environment variables and paths are correctly set up so you can use all the ROS 2 CLI tools.

Running Built-In Nodes

Let’s try launching two example nodes provided by ROS 2:

Copy Code
ros2 run demo_nodes_py talker

This starts a Python node that publishes a message to the /chatter topic every second. Open a new terminal and run:

Copy Code
ros2 run demo_nodes_py listener

The listener node subscribes to the /chatter topic and prints the messages it receives. You’ve just started your first ROS 2 nodes and created a functioning publish/subscribe communication!

Inspecting Topics

Use the following command to see which topics are active:

Copy Code
ros2 topic list

You’ll see several topics, including /chatter, /parameter_events, and /rosout. Each topic represents a data stream that nodes can interact with.

To get more detailed information about a specific topic:

Copy Code
ros2 topic info /chatter

This will show you the message type and how many publishers and subscribers are currently connected to this topic.

You can also inspect live message traffic by echoing a topic:

Copy Code
ros2 topic echo /chatter

This command is invaluable for debugging and understanding what data is being passed around between nodes.

Intro to ROS Part 2: Getting Started with ROS 2 Using the Command Line

Exploring Interfaces

Interfaces define the structure of messages and services in ROS 2. To explore all available interfaces, run:

Copy Code
ros2 interface list

To see the format of a specific message type:

Copy Code
ros2 interface show std_msgs/msg/String

This will show that the String message contains a single data field. You can use this approach to explore more complex message types and understand what kind of data they contain.

Intro to ROS Part 2: Getting Started with ROS 2 Using the Command Line

Visualizing Node Graphs

Run the GUI tool RQT:

Copy Code
rqt

Select Plugins > Introspection > Node Graph. This shows nodes and topics in a visual format. It’s helpful for understanding how nodes interact. Note that you can also enter the following to jump straight to this node graph visualizer:

Copy Code
rqt_graph

Click the refresh button to ensure that the visualizer picks up the running nodes. You should see your /talker and /listener nodes running in the graph.

Intro to ROS Part 2: Getting Started with ROS 2 Using the Command Line

Exploring Services

Press ctrl+c in both terminals to stop the broadcaster and subscriber nodes. Next, we’ll explore services, which use a server/client model. The client sends a request to the server, the server processes the request, and then the server sends back a response to the client.

Let’s now look at how to work with ROS 2 services from the command line. Start a service server:

Copy Code
ros2 run demo_nodes_cpp add_two_ints_server

This node exposes a service that adds two integers together. You can view available services:

Copy Code
ros2 service list

To get detailed information about a specific service:

Copy Code
ros2 service info /add_two_ints

You can see what kind of request and response data is expected using:

Copy Code
ros2 interface show example_interfaces/srv/AddTwoInts

Now, let’s call the service:

Copy Code
ros2 service call /add_two_ints example_interfaces/srv/AddTwoInts "{a: 3, b: 5}"

The result will be displayed in the terminal. This is a great way to test services before integrating them into your own code.

Finally, you can run the matching client:

Copy Code
ros2 run demo_nodes_py add_two_ints_client

This demonstrates how nodes written in different languages (C++ and Python) can communicate using shared message interfaces.

Intro to ROS Part 2: Getting Started with ROS 2 Using the Command Line

Next Steps

You’ve now seen how to:

  • Launch and inspect built-in nodes
  • View and echo topics
  • Explore message and service interfaces
  • Call services from the CLI
  • Use graphical tools like rqt

In the next tutorial, we’ll begin writing our own custom ROS 2 nodes using Python. Understanding these tools will help you test and debug each component as you build more complex applications.

Stay tuned!

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.