Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Product List
LTC3895-Slide3

The 3895 is a 150V input synchronous step-down switching regulator controller that drives an all N-channel MOSFET power stage to deliver up to 20A of output current. Its 40µA operating quiescent current with the output voltage in regulation helps extend the run-time in battery powered applications. This photo at the bottom of the slide shows the critical components required to complete the circuit.

PTM Published on: 2016-07-06